Gets the property information for given file from Design Manager grid.
Visual Basic |
---|
Public Function GetFileAndPropertyDataFromGrid( _ ByRef pVarListFileInfoAndProperties As Variant _ ) As Long |
Imports System.Runtime.InteropServices Public Class Form1 Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click Dim objApp As DesignManager.Application = Nothing Dim objDoc As DesignManager.Document = Nothing Dim strAsmPath As String = "C:\SEWork\00000055_A.asm" Dim strNewPath As String = "C:\SEWork\Newfolder\Revise" Try 'to connect to a running instance of Design Manager Try objApp = Marshal.GetActiveObject("DesignManager.Application") objApp.DisplayAlerts = False objApp.Visible = True Catch ex1 As System.Exception 'SE not running then start it Try objApp = Activator.CreateInstance(Type.GetTypeFromProgID("DesignManager.Application")) objApp.DisplayAlerts = False objApp.Visible = True Catch ex2 As Exception If objApp Is Nothing Then MessageBox.Show("Error starting the DesignManager Manager Application. The error is " + ex1.Message, "Error starting RevMgr.exe", MessageBoxButtons.OK) End If End Try End Try 'Open Assembly file in Design Manager objDoc = objApp.OpenFileInDesignManager(strAsmPath) Dim nAction As DesignManager.DesignManagerAction = DesignManager.DesignManagerAction.SaveAsAction Dim hr As Integer = objApp.SetActionForAllFiles(nAction, strNewPath) Dim fileData As Object = Nothing Dim m_FileNametoPropsMap As Dictionary(Of String, Object) = New Dictionary(Of String, Object) objApp.GetFileAndPropertyDataFromGrid(fileData) Dim numofFiles = fileData.GetLength(0) Dim propInfo1(,) As Object = Nothing Dim FilesNames(numofFiles - 1) As Object Dim ii As Integer If fileData IsNot Nothing Then For ii = 0 To numofFiles - 1 FilesNames(ii) = fileData(ii, 0) m_FileNametoPropsMap.Add(fileData(ii, 0), fileData(ii, 1)) Next End If Dim DocNumincrementor As Integer = 1 Dim RevNumincrementor As Integer = 1 'Dim dt1 As DateTime = Now For Each elemDoc In m_FileNametoPropsMap Dim nPropertiesCount As Integer = elemDoc.Value.GetLength(0) ReDim propInfo1(nPropertiesCount - 1, 1) For ii = 0 To nPropertiesCount - 1 If String.Equals(elemDoc.Value(ii, 0), "Document Number") Then propInfo1(ii, 0) = elemDoc.Value(ii, 0) 'Prop Name propInfo1(ii, 1) = "CX-ZZ-00300_" + DocNumincrementor.ToString() DocNumincrementor = DocNumincrementor + 1 End If If String.Equals(elemDoc.Value(ii, 0), "Revision Number") Then propInfo1(ii, 0) = elemDoc.Value(ii, 0) 'Prop Name propInfo1(ii, 1) = "R" + RevNumincrementor.ToString() RevNumincrementor = RevNumincrementor + 1 End If Next objApp.SetFilePropertyDataToGrid(elemDoc.Key, (propInfo1)) objApp.PerformAction() Exit For Next Catch ex As Exception MsgBox(ex.ToString) Finally objDoc.Close() objDoc = Nothing objApp.Quit() objApp = Nothing End Try End Sub End Class
using System; using System.Windows.Forms; using System.Runtime.InteropServices; public class Form1 { private void Button1_Click(object sender, EventArgs e) { DesignManager.Application objApp = null; DesignManager.Document objDoc = null; string strAsmPath = "C:\\SEWork\\00000055_A.asm"; string strNewPath = "C:\\SEWork\\Newfolder\\Revise"; try { //to connect to a running instance of Design Manager try { objApp = (DesignManager.Application)Marshal.GetActiveObject("DesignManager.Application"); objApp.DisplayAlerts = false; objApp.Visible = true; } catch (System.Exception ex1) { //SE not running then start it try { objApp = Activator.CreateInstance(Type.GetTypeFromProgID("DesignManager.Application")); objApp.DisplayAlerts = false; objApp.Visible = true; } catch (Exception ex2) { if (objApp == null) { MessageBox.Show("Error starting the DesignManager Manager Application. The error is " + ex1.Message, "Error starting RevMgr.exe", MessageBoxButtons.OK); } } } //Open Assembly file in Design Manager objDoc = objApp.OpenFileInDesignManager(strAsmPath); DesignManager.DesignManagerAction nAction = DesignManager.DesignManagerAction.SaveAsAction; int hr = objApp.SetActionForAllFiles(nAction, strNewPath); dynamic fileData = null; Dictionary<string, object> m_FileNametoPropsMap = new Dictionary<string, object>(); objApp.GetFileAndPropertyDataFromGrid(fileData); object numofFiles = fileData.GetLength(0); object[,] propInfo1 = null; object[] FilesNames = new object[numofFiles]; int ii = 0; if (fileData != null) { for (ii = 0; ii < Convert.ToInt32(numofFiles); ii++) { FilesNames[ii] = fileData(ii, 0); m_FileNametoPropsMap.Add(fileData(ii, 0), fileData(ii, 1)); } } int DocNumincrementor = 1; int RevNumincrementor = 1; //Dim dt1 As DateTime = Now foreach (var elemDoc in m_FileNametoPropsMap) { int nPropertiesCount = elemDoc.Value.GetLength(0); propInfo1 = new object[nPropertiesCount, 2]; for (ii = 0; ii < nPropertiesCount; ii++) { if (string.Equals(elemDoc.Value(ii, 0), "Document Number")) { propInfo1[ii, 0] = elemDoc.Value(ii, 0); //Prop Name propInfo1[ii, 1] = "CX-ZZ-00300_" + DocNumincrementor.ToString(); DocNumincrementor = DocNumincrementor + 1; } if (string.Equals(elemDoc.Value(ii, 0), "Revision Number")) { propInfo1[ii, 0] = elemDoc.Value(ii, 0); //Prop Name propInfo1[ii, 1] = "R" + RevNumincrementor.ToString(); RevNumincrementor = RevNumincrementor + 1; } } objApp.SetFilePropertyDataToGrid(elemDoc.Key, (propInfo1)); objApp.PerformAction(); break; } } catch (Exception ex) { MessageBox.Show(ex.ToString()); } finally { objDoc.Close(); objDoc = null; objApp.Quit(); objApp = null; } } public Form1() { SubscribeToEvents(); } private bool EventsSubscribed = false; private void SubscribeToEvents() { if (EventsSubscribed) return; else EventsSubscribed = true; Button1.Click += Button1_Click; Button1.Click += Button1_Click; } }