Enables or disables the display of alerts and messages.
Visual Basic |
---|
Public Property DisplayAlerts As Long |
Option Infer On Imports System Imports System.Runtime.InteropServices Namespace Examples Friend Class Program <STAThread> Shared Sub Main(ByVal args() As String) Dim application As DesignManager.Application = Nothing Try application = New DesignManager.Application() ' Disable alerts. application.DisplayAlerts = 0 ' Enable alerts. application.DisplayAlerts = 1 Catch ex As System.Exception Console.WriteLine(ex) End Try End Sub End Class End Namespace
using System; using System.Runtime.InteropServices; namespace Examples { class Program { [STAThread] static void Main(string[] args) { DesignManager.Application application = null; try { application = new DesignManager.Application(); // Disable alerts. application.DisplayAlerts = 0; // Enable alerts. application.DisplayAlerts = 1; } catch (System.Exception ex) { Console.WriteLine(ex); } } } }