Returns a collection of faces that are intersected by a specified vector.
Property type
Read-only property
Syntax
Visual Basic
Public Property FacesByRay( _
ByVal xOrigin As Double, _
ByVal yOrigin As Double, _
ByVal Zorigin As Double, _
ByVal Xdir As Double, _
ByVal Ydir As Double, _
ByVal Zdir As Double _
) As Object
Parameters
xOrigin
yOrigin
Zorigin
Xdir
Ydir
Zdir
Remarks
The result of the FacesByRay property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used.