Option Infer On
Imports System
Imports System.Collections.Generic
Imports System.Runtime.InteropServices
Namespace Examples
Friend Class Program
<STAThread>
Shared Sub Main(ByVal args() As String)
Dim application As SolidEdgeFramework.Application = Nothing
Dim partDocument As SolidEdgePart.PartDocument = Nothing
Dim models As SolidEdgePart.Models = Nothing
Dim model As SolidEdgePart.Model = Nothing
Try
' See "Handling 'Application is Busy' and 'Call was Rejected By Callee' errors" topic.
OleMessageFilter.Register()
' Attempt to connect to a running instance of Solid Edge.
application = DirectCast(Marshal.GetActiveObject("SolidEdge.Application"), SolidEdgeFramework.Application)
partDocument = TryCast(application.ActiveDocument, SolidEdgePart.PartDocument)
models = partDocument.Models
model = models.Item(1)
Catch ex As System.Exception
Console.WriteLine(ex)
Finally
OleMessageFilter.Unregister()
End Try
End Sub
End Class
End Namespace
using System;
using System.Collections.Generic;
using System.Runtime.InteropServices;
namespace Examples
{
class Program
{
[STAThread]
static void Main(string[] args)
{
SolidEdgeFramework.Application application = null;
SolidEdgePart.PartDocument partDocument = null;
SolidEdgePart.Models models = null;
SolidEdgePart.Model model = null;
try
{
// See "Handling 'Application is Busy' and 'Call was Rejected By Callee' errors" topic.
OleMessageFilter.Register();
// Attempt to connect to a running instance of Solid Edge.
application = (SolidEdgeFramework.Application)Marshal.GetActiveObject("SolidEdge.Application");
partDocument = application.ActiveDocument as SolidEdgePart.PartDocument;
models = partDocument.Models;
model = models.Item(1);
}
catch (System.Exception ex)
{
Console.WriteLine(ex);
}
finally
{
OleMessageFilter.Unregister();
}
}
}
}