Class Module | Description |
---|---|
Body | Provides a set of interfaces that allow you to access the topological and sense data that is related to the object. |
BSplineCurve | Describes the 3-D B-Spline curve. |
BSplineSurface | Describes the B-Spline surface of the faces of a solid. |
Circle | Represents the circle surface geometry to provide access to information about the faces of a solid. |
Cone | Represents the cone surface geometry to provide access to information about the faces of a solid. |
Curve | Represents an occurrence of a curve topological entity. |
CurveBody | Represents an instance of a construction surface. |
CurvePath | Represents an occurrence of a collection of curves presented in sequential order. |
CurvePaths | Represents a collection of CurvePath objects. |
Curves | Represents a collection of Curve objects. |
CurveVertex | Holds the topological position of the endpoint of an Edge. |
CurveVertices | Represents a collection of Vertices. |
Cylinder | Represents the cylinder surface geometry to provide access to information about the faces of a solid. |
Edge | Represents the elemental piece of the 3-D geometry information for the boundaries of a Face. |
Edges | Represents a collection of Edges. |
EdgeUse | Represents the use of a given Edge in a loop. |
EdgeUses | Represents a collection of EdgeUses. |
Ellipse | Represents the ellipse surface geometry to provide access to information about the faces of a solid. |
Face | Represents the elemental piece of surface data that makes up the body. |
Faces | Represents a collection of Faces. |
Line | Describes a Line in 3-D space. |
Loop | Represents a closed contour on a given Face. |
Loops | Represents a collection of Loops. |
MeshSurface | Represents the mesh surface geometry to provide access to information about the faces of a solid. |
ParamBSplineCurve | Describes the 2-D B-Spline curve. |
Plane | Represents the plane surface geometry to provide access to information about the faces of a solid. |
PLine | Describes a Poly Line in 3-D space. |
Shell | Represents a set of connected Faces. |
Shells | Represents a collection of Shells. |
Sphere | Represents the sphere surface geometry to provide access to information about the faces of a solid. |
Torus | Represents the torus surface geometry to provide access to information about the faces of a solid. |
Vertex | Holds the topological position of the endpoint of an Edge. |
Vertices | Represents a collection of Vertices. |
Enumeration | Description |
---|---|
FeatureTopologyQueryTypeConstants | Feature Topology Query Type Constants |
GNTTypePropertyConstants | GNT Type Property Constants |
MeshHoleFillShapeType | This datatype specifies the shape required when mesh holes are filled |
SmartCollectionTypeConstants | Smart Collection Type Constants |
TopologyCollectionTypeConstants | Topology Collection Type Constants |