Solid Edge FrameworkSupport Type Library
GostWeldSymbol Object
Members 
Description
Specifies all unique GOST weld types necessary in the fabrication of the weldment.
Object Model
GostWeldSymbol ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFeatureSelectedFromPFEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDisplayData ObjectDimStyle Object
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheets As SolidEdgeDraft.Sheets = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objGostWelds As SolidEdgeFrameworkSupport.GostWeldSymbols = Nothing
        Dim objGostWeld As SolidEdgeFrameworkSupport.GostWeldSymbol = Nothing
        Dim objLines As SolidEdgeFrameworkSupport.Lines2d = Nothing
        Dim objLine1 As SolidEdgeFrameworkSupport.Line2d = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
            objApplication.Visible = True
            objDocuments = objApplication.Documents
            objDraftDocument = objDocuments.Add("SolidEdge.DraftDocument")
            objSheet = objDraftDocument.ActiveSheet
            objLines = objSheet.Lines2d
            objGostWelds = objSheet.GostWeldSymbols

            'Add a horizontal line
            objLine1 = objLines.AddBy2Points(0.1, 0.1, 0.3, 0.1)

            'Create GOST weld
            objGostWeld = objGostWelds.AddByTerminator(objLine1, 0.125, 0.1, 0.0, True)

            objGostWeld.AddVertex(0.2, 0.05, 0)

            'Set the properties for GOST weld symbol.
            objGostWeld.TextScale = 10
            objGostWeld.Leader = True
            objGostWeld.BreakLine = True
            objGostWeld.PermanentJoint = True
            objGostWeld.PermanentJointType = SolidEdgeFrameworkSupport.DimGostWeldPermanentJointTypeConstants.igDimGostWeldPermJointStitch
            objGostWeld.AboveBreakLineText = "Text Above"
            objGostWeld.BelowBreakLineText = "Below"
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
using System.IO;
using System.Runtime.InteropServices;

internal static class Example
{
    [STAThread()]
    public static void Main()
    {
        SolidEdgeFramework.Application objApplication = null;
        SolidEdgeFramework.Documents objDocuments = null;
        SolidEdgeDraft.DraftDocument objDraftDocument = null;
        SolidEdgeDraft.Sheets objSheets = null;
        SolidEdgeDraft.Sheet objSheet = null;
        SolidEdgeFrameworkSupport.GostWeldSymbols objGostWelds = null;
        SolidEdgeFrameworkSupport.GostWeldSymbol objGostWeld = null;
        SolidEdgeFrameworkSupport.Lines2d objLines = null;
        SolidEdgeFrameworkSupport.Line2d objLine1 = null;

        try
        {
            OleMessageFilter.Register();

            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"));
            objApplication.Visible = true;
            objDocuments = objApplication.Documents;
            objDraftDocument = objDocuments.Add("SolidEdge.DraftDocument");
            objSheet = objDraftDocument.ActiveSheet;
            objLines = objSheet.Lines2d;
            objGostWelds = objSheet.GostWeldSymbols;

            //Add a horizontal line
            objLine1 = objLines.AddBy2Points(0.1, 0.1, 0.3, 0.1);

            //Create GOST weld
            objGostWeld = objGostWelds.AddByTerminator(objLine1, 0.125, 0.1, 0.0, true);

            objGostWeld.AddVertex(0.2, 0.05, 0);

            //Set the properties for GOST weld symbol.
            objGostWeld.TextScale = 10;
            objGostWeld.Leader = true;
            objGostWeld.BreakLine = true;
            objGostWeld.PermanentJoint = true;
            objGostWeld.PermanentJointType = SolidEdgeFrameworkSupport.DimGostWeldPermanentJointTypeConstants.igDimGostWeldPermJointStitch;
            objGostWeld.AboveBreakLineText = "Text Above";
            objGostWeld.BelowBreakLineText = "Below";
        }
        catch (Exception ex)
        {
            Console.WriteLine(ex.Message);
        }
        finally
        {
            OleMessageFilter.Revoke();
        }
    }
}
See Also

GostWeldSymbol Members  | Solid Edge ST2 - What's New