Solid Edge Assembly Type Library
VirtualComponent Object Members
Overview 
Public Methods
Public Method DeleteDelete this Virtual Component and all its Virtual Component occurrences.
Public Method GetGeometry
Public Method RemoveGeometry
Public Method SetGeometry
Public Method UpdateComponent
Public Properties
Public Property Application
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameSpecify or retrieve the name of the Virtual Component.
Public Property Parent
Public Property PropertiesRetrieve the collection of properties for this Virtual Component.
Public Property PublishPathSpecify or retrieve the path to the directory in which to create the document file when the Virtual Component is published.
Public Property TemplateNameSpecify or retrieve the template file name to use to create the document file when the Virtual Component is published.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VirtualComponentOccurrencesRetrieve the collection of Virtual Component occurrences for this Virtual Component.
Public Property VirtualComponentTypeRetrieve the Virtual Component type which may be seVirtualComponentType_Assembly, seVirtualComponentTypeType_Part, or  seVirtualComponentType_Sheetmetal.
See Also

VirtualComponent Object  | Solid Edge V17 - What's New