Solid Edge Assembly Type Library
CurveSegment Object
Members 
Description
Represents an occurrence of a curve segment element.
Object Model
CurveSegment ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFeatureSelectedFromPFEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Remarks
Because you define it with input segments, specified keypoints, and derivative magnitudes, it allows for a smoother, more free-flowing tube or wire than the LineSegment or ArcSegment objects.
See Also

CurveSegment Members