Solid Edge Assembly Type Library : AssemblyFeaturesPattern Object |
AddSuppressionVariable | |
Delete | Deletes the referenced object. |
DeleteSuppressionVariable | |
GetParentFeatures | |
GetPatternType | |
GetProfile | |
GetSuppressionVariable | |
HasSuppressionVariable | |
Range | Returns the high and low range values for the referenced object. |
RollToFeature | This method rolls the referenced object back to a specified feature. |
SetParentFeatures | |
SetPatternType | |
SetProfile |
Application | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. The result of the Edges property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. |
EdgesForScopePart | |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. The result of the Faces property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FacesByRayForScopePart | |
FacesForScopePart | |
Name | Returns the name of the referenced object. |
Parent | |
Status | |
Suppress | Temporarily suppresses the referenced object. |