Solid Edge Assembly Type Library
AsmRefPlanes Collection Members
Overview 
Public Methods
Public Method AddAngularByAngleCreates a reference plane at an angle to an existing reference plane or face and through an edge or an intersection of two faces.
Public Method AddBy3PointsAdds a reference plane by 3 points.
Public Method AddNormalToCurveAtArcLengthRatioAdds a reference plane normal to a curve at the specified arc length ratio.
Public Method AddNormalToCurveAtDistanceAlongCurveAdds a reference plane normal to a curve at a specified distance along the curve.
Public Method AddNormalToCurveAtKeyPointAdds a reference plane normal to a curve at the specified keypoint.
Public Method AddParallelByDistanceCreates a RefPlane object that is parallet to another plane.
Public Method ItemThe items in a collection.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property CountReturns the number of objects in the referenced collection.
Public Property ParentReturns the parent object for the referenced object.
Public Property Visible
See Also

AsmRefPlanes Collection