VB.NET implementation of OleMessageFilter |
Copy Code |
---|---|
Imports System.Runtime.InteropServices Imports System.Threading Public Class OleMessageFilter Implements IOleMessageFilter Public Shared Sub Register() Dim newFilter As IOleMessageFilter = New OleMessageFilter() Dim oldFilter As IOleMessageFilter = Nothing Dim iRetVal As Integer If (Thread.CurrentThread.GetApartmentState() = ApartmentState.STA) Then iRetVal = CoRegisterMessageFilter(newFilter, oldFilter) Else Throw New COMException("Unable to register message filter because the current thread apartment state is not STA.") End If End Sub Public Shared Sub Revoke() Dim oldFilter As IOleMessageFilter = Nothing CoRegisterMessageFilter(Nothing, oldFilter) End Sub Private Function HandleInComingCall(ByVal dwCallType As Integer, _ ByVal hTaskCaller As System.IntPtr, _ ByVal dwTickCount As Integer, _ ByVal lpInterfaceInfo As System.IntPtr) _ As Integer Implements IOleMessageFilter.HandleInComingCall Return SERVERCALL.SERVERCALL_ISHANDLED End Function Private Function RetryRejectedCall(ByVal hTaskCallee As System.IntPtr, _ ByVal dwTickCount As Integer, _ ByVal dwRejectType As Integer) _ As Integer Implements IOleMessageFilter.RetryRejectedCall If dwRejectType = SERVERCALL.SERVERCALL_RETRYLATER Then Return 99 End If Return -1 End Function Private Function MessagePending(ByVal hTaskCallee As System.IntPtr, _ ByVal dwTickCount As Integer, _ ByVal dwPendingType As Integer) _ As Integer Implements IOleMessageFilter.MessagePending Return PENDINGMSG.PENDINGMSG_WAITDEFPROCESS End Function <DllImport("Ole32.dll")> _ Private Shared Function CoRegisterMessageFilter(ByVal newFilter As IOleMessageFilter, _ ByRef oldFilter As IOleMessageFilter) _ As Integer End Function End Class Enum SERVERCALL SERVERCALL_ISHANDLED = 0 SERVERCALL_REJECTED = 1 SERVERCALL_RETRYLATER = 2 End Enum Enum PENDINGMSG PENDINGMSG_CANCELCALL = 0 PENDINGMSG_WAITNOPROCESS = 1 PENDINGMSG_WAITDEFPROCESS = 2 End Enum <ComImport(), _ Guid("00000016-0000-0000-C000-000000000046"), _ InterfaceTypeAttribute(ComInterfaceType.InterfaceIsIUnknown)> _ Interface IOleMessageFilter <PreserveSig()> _ Function HandleInComingCall(ByVal dwCallType As Integer, _ ByVal hTaskCaller As IntPtr, _ ByVal dwTickCount As Integer, _ ByVal lpInterfaceInfo As IntPtr) _ As Integer <PreserveSig()> _ Function RetryRejectedCall(ByVal hTaskCallee As IntPtr, _ ByVal dwTickCount As Integer, _ ByVal dwRejectType As Integer) _ As Integer <PreserveSig()> _ Function MessagePending(ByVal hTaskCallee As IntPtr, _ ByVal dwTickCount As Integer, _ ByVal dwPendingType As Integer) _ As Integer End Interface |