C# implementation of OleMessageFilter |
Copy Code |
---|---|
using System; using System.Runtime.InteropServices; using System.Threading; namespace SolidEdge.SDK { class OleMessageFilter : IOleMessageFilter { public static void Register() { IOleMessageFilter newFilter = new OleMessageFilter(); IOleMessageFilter oldFilter = null; if (Thread.CurrentThread.GetApartmentState() == ApartmentState.STA) { CoRegisterMessageFilter(newFilter, out oldFilter); } else { throw new COMException("Unable to register message filter because the current thread apartment state is not STA."); } } public static void Revoke() { IOleMessageFilter oldFilter = null; CoRegisterMessageFilter(null, out oldFilter); } int IOleMessageFilter.HandleInComingCall( int dwCallType, System.IntPtr hTaskCaller, int dwTickCount, System.IntPtr lpInterfaceInfo) { return (int)SERVERCALL.SERVERCALL_ISHANDLED; } int IOleMessageFilter.RetryRejectedCall( System.IntPtr hTaskCallee, int dwTickCount, int dwRejectType) { if (dwRejectType == (int)SERVERCALL.SERVERCALL_RETRYLATER) { return 99; } return -1; } int IOleMessageFilter.MessagePending( System.IntPtr hTaskCallee, int dwTickCount, int dwPendingType) { return (int)PENDINGMSG.PENDINGMSG_WAITDEFPROCESS; } [DllImport("Ole32.dll")] private static extern int CoRegisterMessageFilter( IOleMessageFilter newFilter, out IOleMessageFilter oldFilter); } enum SERVERCALL { SERVERCALL_ISHANDLED = 0, SERVERCALL_REJECTED = 1, SERVERCALL_RETRYLATER = 2 } enum PENDINGMSG { PENDINGMSG_CANCELCALL = 0, PENDINGMSG_WAITNOPROCESS = 1, PENDINGMSG_WAITDEFPROCESS = 2 } [ComImport(), Guid("00000016-0000-0000-C000-000000000046"), InterfaceTypeAttribute(ComInterfaceType.InterfaceIsIUnknown)] interface IOleMessageFilter { [PreserveSig] int HandleInComingCall( int dwCallType, IntPtr hTaskCaller, int dwTickCount, IntPtr lpInterfaceInfo); [PreserveSig] int RetryRejectedCall( IntPtr hTaskCallee, int dwTickCount, int dwRejectType); [PreserveSig] int MessagePending( IntPtr hTaskCallee, int dwTickCount, int dwPendingType); } } |