StructureEditor Namespace
SetSaveAsSelected Method
Specifies the item id of the document on which the save as action is to be set.
Specifies the revision of the document on which the save as action is to be set.
Specifies the Name of the file on which the save as action is to be set.
Description
This API is used to set save as action on a selected solid edge file in the structure editor.
Syntax
Visual Basic
Public Function SetSaveAsSelected( _
   ByVal bstrItemId As String, _
   ByVal bstrItemRev As String, _
   ByVal bstrDataSetFileName As String _
) As Long
Parameters
bstrItemId
Specifies the item id of the document on which the save as action is to be set.
bstrItemRev
Specifies the revision of the document on which the save as action is to be set.
bstrDataSetFileName
Specifies the Name of the file on which the save as action is to be set.
Remarks
Call this API after calling open() API. Because for calling this API a solid edge file needs to be opened in the structure editor application. If the action is set without opening a solid edge file in the application then nothing will happen. If user wants to select multiple files for save as then the above code needs to be called multiple times.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As StructureEditor.Application = Nothing
        Dim objStructureEditor As StructureEditor.SEECStructureEditor = Nothing
        Dim strItemId As String
        Dim strItemRev As String
        Dim strFileName As String
        Dim strRevisionRule As String
        Dim strFolderName As String

        Try
            OleMessageFilter.Register()

            ' Start structure editor application
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("StructureEditor.Application"))
            objStructureEditor = objApplication.SEECStructureEditor
            objApplication.Visible = True

            strItemId = "081691"
            strItemRev = "A"
            strFileName = "a.asm"
            strRevisionRule = "Latest Working"
            strFolderName = ""

            If objStructureEditor.Open(strItemId, strItemRev, strFileName, strRevisionRule, strFolderName) = 0 Then
                objStructureEditor.SetSaveAsSelected(strItemId, strItemRev, strFileName)
            End If
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            If Not objApplication Is Nothing Then
                ' Kill the instance of structure editor created
                objApplication.Quit()
            End If

            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

ISEECStructureEditor Object  | ISEECStructureEditor Members