Imports System.IO
Imports System.Runtime.InteropServices
Module Example
<STAThread()> _
Sub Main()
Dim objApplication As StructureEditor.Application = Nothing
Dim objStructureEditor As StructureEditor.SEECStructureEditor = Nothing
Dim strItemId As String
Dim strItemRev As String
Dim strFileName As String
Dim strRevisionRule As String
Dim strFolderName As String
Try
OleMessageFilter.Register()
' Start structure editor application
objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("StructureEditor.Application"))
objStructureEditor = objApplication.SEECStructureEditor
objApplication.Visible = True
strItemId = "081691"
strItemRev = "A"
strFileName = "a.asm"
strRevisionRule = "Latest Working"
strFolderName = ""
If objStructureEditor.Open(strItemId, strItemRev, strFileName, strRevisionRule, strFolderName) = 0 Then
objStructureEditor.SetReviseAll()
End If
Catch ex As Exception
Console.WriteLine(ex.Message)
Finally
If Not objApplication Is Nothing Then
' Kill the instance of structure editor created
objApplication.Quit()
End If
OleMessageFilter.Revoke()
End Try
End Sub
End Module