Solid Edge Part Type Library
StartOffset Property
Collapse All
Expand All
Solid Edge Part Type Library
>
PartStitchWeld Object
: StartOffset Property
Description
Sets and returns the length of material to remove from the start of the weld bead for the referenced PartStitchWeld object.
Property type
Read-write property
Syntax
Visual Basic
Public Property StartOffset As Double
See Also
PartStitchWeld Object
|
PartStitchWeld Members