Solid Edge Geometry Type Library
Item Method
Variant (input) index.
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal index As Variant _
) As Object
Parameters
index
Variant (input) index.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objExtrudedProtrusions As SolidEdgePart.ExtrudedProtrusions = Nothing
        Dim objExtrudedProtrusion As SolidEdgePart.ExtrudedProtrusion = Nothing
        Dim objFaces As SolidEdgeGeometry.Faces = Nothing
        Dim objFace As SolidEdgeGeometry.Face = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument
            objModels = objPartDocument.Models
            objModel = objModels.Item(1)
            objExtrudedProtrusions = objModel.ExtrudedProtrusions
            objExtrudedProtrusion = objExtrudedProtrusions.Item(1)
            objFaces = objExtrudedProtrusion.Faces(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll)
            objFace = objFaces.Item(1)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub

End Module
See Also

Faces Collection  | Faces Members