The movie's bit rate (bits per second). Must be greater than 0. Higher values give better quality but larger file sizes. A value of 2500000 or above is recommended.
Property type
Read-write property
Syntax
Visual Basic
Public Property MovieBitRate As ULong
Remarks
Returns or sets the bit rate for the movie. A higher bit rate will give a better quality movie, but the file size will be bigger. A default bit rate is computed based on frame rate and other factors. Only available for the WMV format.