Solid Edge Framework Type Library
ApplyNamedView Method
Specify Name of the view object as string.
Description
Apply a named view.
Syntax
Visual Basic
Public Sub ApplyNamedView( _
   ByVal Name As Variant _
) 
Parameters
Name
Specify Name of the view object as string.
Remarks
This API takes a string as an argument and applies the view based on its name.
Example
Imports System.Runtime.InteropServices
Public Class Form1

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDoc As SolidEdgePart.PartDocument = Nothing
        Dim Obj1 As Object = Nothing
        Try
            ' Get application 
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
                objApplication.Visible = True
            End If

            If objPartDoc Is Nothing Then
                objPartDoc = objPartDoc.Documents.Add("SolidEdge.PartDocument")
            End If

            ' The methods take variants (objects) in order to allow for expansion in further projects but at this moment they will only take strings. 
            Obj1 = "TestView"
            Dim window As SolidEdgeFramework.Window = objPartDoc.Windows.Item(1)
            Dim view As SolidEdgeFramework.View
            view = window.View
            view.SaveCurrentView(Obj1)
            view.ApplyNamedView(Obj1)
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try

    End Sub
End Class
See Also

View Object  | View Members