Solid Edge Framework Type Library
SetAnalysisParameters Method
Description
Sets the analysis parameters of the referenced ViewStyle object.
Syntax
Visual Basic
Public Sub SetAnalysisParameters( _
   ByVal eState As SeAnalysisStateType, _
   Optional ByVal eMode As SeAnalysisModeType = seAnalysisModeDefault, _
   Optional ByVal QualityScale As Variant, _
   Optional ByVal Arg1 As Variant, _
   Optional ByVal Arg2 As Variant, _
   Optional ByVal Arg3 As Variant, _
   Optional ByVal Arg4 As Variant _
) 
Parameters
eState
ValueDescription
seAnalysisStateGlobalGlobal Analysis State
seAnalysisStateLocalLocal Analysis State
seAnalysisStateNoneNo Analysis State
eMode
ValueDescription
seAnalysisModeCurvatureColorCurvature Color Analysis Mode
seAnalysisModeDefaultDefault/propogated Analysis Mode
seAnalysisModeDraftAngleCurvature Color Analysis Mode
seAnalysisModeZebraStripeLinearLinear Zebra Stripe Analysis Mode
seAnalysisModeZebraStripeReflectionReflection Zebra Stripe Analysis Mode
seAnalysisModeZebraStripeSphericalSpherical Zebra Stripe Analysis Mode
QualityScale
Arg1
Arg2
Arg3
Arg4
See Also

ViewStyle Object  | ViewStyle Members