Solid Edge Framework Type Library
GetSkyboxOrientation Method
Description
Returns the orientation of the skybox used in the referenced ViewStyle object.
Syntax
Visual Basic
Public Sub GetSkyboxOrientation( _
   ByRef pfxDirection As Single, _
   ByRef pfyDirection As Single, _
   ByRef pfzDirection As Single, _
   ByRef pfxUp As Single, _
   ByRef pfyUp As Single, _
   ByRef pfzUp As Single, _
   ByRef pfFieldOfView As Single _
) 
Parameters
pfxDirection
pfyDirection
pfzDirection
pfxUp
pfyUp
pfzUp
pfFieldOfView
See Also

ViewStyle Object  | ViewStyle Members  | Solid Edge ST4 - What's New