Solid Edge Framework Type Library
UnitTypeConstants Enumeration
Description
Unit Type Constants
Members
MemberValueDescription
igUnitAmountOfSubstance8Unit Type - Amount of Substance
igUnitAngle2Unit Type - Angle
igUnitAngularAcceleration10Unit Type - Angular Acceleration
igUnitAngularMomentum11Unit Type - Angular Momentum
igUnitAngularVelocity12Unit Type - Angular Velocity
igUnitArea13Unit Type - Area
igUnitBodyForce14Unit Type - Body Force
igUnitCoefficientOfThermalExpansion15Unit Type - Coefficient of Thermal Expansion
igUnitDensity16Unit Type - Density
igUnitDistance1Unit Type - Distance
igUnitDynamicViscosity54Unit Type - Dynamic Viscosity
igUnitElectricalCapacitance17Unit Type - Electrical Capacitance
igUnitElectricalConductance18Unit Type - Electrical Conductance
igUnitElectricalFieldStrength19Unit Type - Electrical Fieldf Strength
igUnitElectricalInductance20Unit Type - Electrical Inductance
igUnitElectricalPotential21Unit Type - Electrical Potential
igUnitElectricalResistance22Unit Type - Electrical Resistance
igUnitElectricCharge6Unit Type - Electrical Charge
igUnitEnergy23Unit Type - Energy
igUnitEnergyDensity60Unit Type - EnergyDensity
igUnitEntropy24Unit Type - Entropy
igUnitFilmCoefficient25Unit Type - Film Coefficient
igUnitForce26Unit Type - Force
igUnitForcePerArea27Unit Type - Force Per Area
igUnitForcePerDistance28Unit Type - Force Per Distance
igUnitFrequency29Unit Type - Frequency
igUnitHeatCapacity30Unit Type - Heat Capacity
igUnitHeatFluxPerArea31Unit Type - Heat Flux Per Area
igUnitHeatFluxPerDistance32Unit Type - Heat Flux Per Distance
igUnitHeatGeneration62Unit Type - Heat Generation
igUnitHeatSource33Unit Type - Heat Source
igUnitIlluminance34Unit Type - Illuminance
igUnitKinematicViscosity55Unit Type - Kinematic Viscosity
igUnitLinearAcceleration35Unit Type - Linear Acceleration
igUnitLinearPerAngular36Unit Type - Linear Per Angular
igUnitLinearVelocity37Unit Type - Linear Velocity
igUnitLuminousFlux38Unit Type - Luminous Flux
igUnitLuminousIntensity7Unit Type - Luminous Intensity
igUnitMagneticFieldStrength39Unit Type - Magnetic Field Strength
igUnitMagneticFlux40Unit Type - Magnetic Flux
igUnitMagneticFluxDensity41Unit Type - Magnetic Flux Density
igUnitMass3Unit Type - Mass
igUnitMassFlowRate42Unit Type - Mass Flow Rate
igUnitMassMomentOfInertia43Unit Type - Mass Moment of Inertia
igUnitMassPerArea44Unit Type - Mass Per Area
igUnitMassPerLength45Unit Type - Mass Per Length
igUnitMomentum46Unit Type - Momentum
igUnitPerDistance47Unit Type - Per Distance
igUnitPower48Unit Type - Power
igUnitPressure61Unit Type - Pressure
igUnitQuantityOfElectricity49Unit Type - Quantity of Electricity
igUnitRadiantIntensity50Unit Type - Radiant Intensity
igUnitRotationalStiffness51Unit Type - Rotation Stiffness
igUnitScalar58Unit Type - Scalar
igUnitSecondMomentOfArea52Unit Type - Second Moment of Area
igUnitSolidAngle9Unit Type - Solid Angle
igUnitTemperature5Unit Type - Temperature
igUnitTemperatureGradient63Unit Type - Temperature Gradient
igUnitThermalConductivity53Unit Type - Thermal Conductivity
igUnitTime4Unit Type - Time
igUnitTorque59Unit Type - Torque
igUnitVolume56Unit Type - Volume
igUnitVolumeFlowRate57Unit Type - Volume Flow Rate
See Also

Solid Edge ST5 - What's New  | Solid Edge ST2 - What's New