Solid Edge Framework Type Library
UnitOfMeasure Object Members
Overview
Collapse All
Expand All
Solid Edge Framework Type Library
: UnitOfMeasure Object
Public Properties
Precision
This read-write Long property sets and returns the unit precision for the referenced UnitOfMeasure object.
Type
Specifies the type of the object being referenced.
Units
Sets and returns the units in which the line width is defined.
See Also
UnitOfMeasure Object