Solid Edge Framework Type Library
TextCharStyles Collection
Members
Collapse All
Expand All
Solid Edge Framework Type Library
: TextCharStyles Collection
Description
A collection of TextCharStyle objects.
Remarks
The Add method creates a new TextCharStyle object from a copy of an existing one. To customize this object, set the TextCharStyle object's properties as needed to set the characteristics.
See Also
TextCharStyles Members