Solid Edge Framework Type Library
OnUndoCheckOutDocuments Method

The variant array which contains the file list to be UndoCheckOut.

Description
Undo checkout files in the cache
Syntax
Visual Basic
Public Sub OnUndoCheckOutDocuments( _
   ByRef psaCacheFiles() As Variant _
) 
Parameters
psaCacheFiles

The variant array which contains the file list to be UndoCheckOut.

Example
Private Sub Command1_Click()
    On Error Resume Next
    Dim objApplication As SolidEdgeFramework.Application
    Dim objSolidEdgeTCE As SolidEdgeFramework.SolidEdgeTCE
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objSolidEdgeTCE = objApplication.SolidEdgeTCE

    Dim varInputList(1) As Variant
    varInputList(0) = "F:\016954.asm"
    varInputList(1) = "F:\016973.asm"
    Call objSolidEdgeTCE.OnUndoCheckOutDocuments(varInputList)

    Set objSolidEdgeTCE = Nothing
    Set objApplication = Nothing
End Sub

See Also

SolidEdgeTCE Object  | SolidEdgeTCE Members  | Solid Edge ST - What's New