Solid Edge Framework Type Library
OnSynchronizeFile Method

The variant array which contains the file list to be Synchronize.

Description
Synchronize files from cache
Syntax
Visual Basic
Public Sub OnSynchronizeFile( _
   ByRef psaSynchFiles() As Variant, _
   Optional ByVal enumSyncOption As SyncOption = SEECSyncAll _
) 
Parameters
psaSynchFiles

The variant array which contains the file list to be Synchronize.

enumSyncOption
ValueDescription
SEECSyncAll 
SEECSyncOne 
Example
Private Sub Command1_Click()
    On Error Resume Next
    Dim objApplication As SolidEdgeFramework.Application
    Dim objSolidEdgeTCE As SolidEdgeFramework.SolidEdgeTCE
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objSolidEdgeTCE = objApplication.SolidEdgeTCE

    Dim varInputList(1) As Variant
    varInputList(0) = "F:\016954.asm"
    varInputList(1) = "F:\016973.asm"
    
    Call objSolidEdgeTCE.OnSynchronizeFile(varInputList)

    Set objSolidEdgeTCE = Nothing
    Set objApplication = Nothing
End Sub

See Also

SolidEdgeTCE Object  | SolidEdgeTCE Members  | Solid Edge ST - What's New