Solid Edge Framework Type Library
GetUserLogMessages Method
Returns the user log messages generated during a session.
Description
Gives the list of userlog messages
Syntax
Visual Basic
Public Sub GetUserLogMessages( _
   ByRef pvarUserLogMessages As Variant _
) 
Parameters
pvarUserLogMessages
Returns the user log messages generated during a session.
Example
Option Explicit

Sub Example()
    Dim objApplication As SolidEdgeFramework.Application
    Dim objTCE As SolidEdgeFramework.SolidEdgeTCE
    Dim pusermessages As Variant
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objTCE = objApplication.SolidEdgeTCE

    Call objTCE.GetUserLogMessages(pusermessages)
    
    If Not objApplication Is Nothing Then
        Call objApplication.Quit
    End If
    
    Set objTCE = Nothing
    Set objApplication = Nothing
End Sub
See Also

SolidEdgeTCE Object  | SolidEdgeTCE Members  | Solid Edge ST - What's New