Solid Edge Framework Type Library
GetProjectsForLoggedInUSer Method
Names of Projects in variant (out).
Description
Returns the projects for given user.
Syntax
Visual Basic
Public Sub GetProjectsForLoggedInUSer( _
   ByRef pvarListOfUserProjects As Variant, _
   ByRef pvarListOfUserProjectUIDs As Variant _
) 
Parameters
pvarListOfUserProjects
Names of Projects in variant (out).
pvarListOfUserProjectUIDs
Example
Option Explicit

Sub Example()
    Dim objApplication As SolidEdgeFramework.Application
    Dim objTCE As SolidEdgeFramework.SolidEdgeTCE
    Dim pListofProjects As Variant
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objTCE = objApplication.SolidEdgeTCE

    Call objTCE.GetProjectsForLoggedInUSer(pListofProjects)
    
    If Not objApplication Is Nothing Then
        Call objApplication.Quit
    End If
    
    Set objTCE = Nothing
    Set objApplication = Nothing
End Sub
See Also

SolidEdgeTCE Object  | SolidEdgeTCE Members  | Solid Edge ST3 - What's New