Solid Edge Framework Type Library
ReviseToInsightXT Method
Specifies the item-id of the item.
Specifies the item-rev of the item.
DataSetName of the file.
Revision Rule of the file.
Name of the folder where the new file supposed to save.
The old and new data such as ItemId,Rev,FileName.
Description
Create a new revision of a file
Syntax
Visual Basic
Public Sub ReviseToInsightXT( _
   ByVal bstrItemId As String, _
   ByVal bstrItemRev As String, _
   ByVal bstrDataSetFileName As String, _
   ByVal bstrRevisionRule As String, _
   ByVal bstrFolderName As String, _
   ByRef pvarListOldAndNewItemIDRevsFileNames As Variant _
) 
Parameters
bstrItemId
Specifies the item-id of the item.
bstrItemRev
Specifies the item-rev of the item.
bstrDataSetFileName
DataSetName of the file.
bstrRevisionRule
Revision Rule of the file.
bstrFolderName
Name of the folder where the new file supposed to save.
pvarListOldAndNewItemIDRevsFileNames
The old and new data such as ItemId,Rev,FileName.
Example
Private Sub Command1_Click()
    On Error Resume Next
    Dim objApplication As SolidEdgeFramework.Application
    Dim objSolidEdgeInsightXT  As SolidEdgeFramework.SolidEdgeInsightXT
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objSolidEdgeInsightXT = objApplication.SolidEdgeInsightXT

    Dim FileItemID As String
    Dim FileItemRevID As String
    Dim FileDataSetName As String
    Dim FileRevisionRule As String
    Dim FolderName As String
    Dim pListOldAndNewItemIDRevsFileNames As Variant
    
    FileItemID = "020670"
    FileItemRevID = "A"
    FileDataSetName = "020670.par"
    FileRevisionRule = ""
    FolderName = ""

    Call objSolidEdgeInsightXT.ReviseToInsightXT(FileItemID, _
        FileItemRevID, _
        FileDataSetName, _
        FileRevisionRule, _
        FolderName, _
        pListOldAndNewItemIDRevsFileNames)

    Set objSolidEdgeInsightXT = Nothing
    Set objApplication = Nothing
End Sub
See Also

SolidEdgeInsightXT Object  | SolidEdgeInsightXT Members  | Solid Edge ST4 - What's New