Solid Edge Framework Type Library
GetListOfFilesFromInsightXTServer Method
Specifies the Item Id of the file.
Specifies the Revision of the file.
File Names.
Number of files.
Description
Get list of files from server.
Syntax
Visual Basic
Public Sub GetListOfFilesFromInsightXTServer( _
   ByVal bstrDirctFileItemId As String, _
   ByVal bstrDirctFileItemRevId As String, _
   ByRef vFileNames As Variant, _
   ByRef nFiles As Long _
) 
Parameters
bstrDirctFileItemId
Specifies the Item Id of the file.
bstrDirctFileItemRevId
Specifies the Revision of the file.
vFileNames
File Names.
nFiles
Number of files.
Example
Private Sub Command1_Click()
    On Error Resume Next
    Dim objApplication As SolidEdgeFramework.Application
    Dim objSolidEdgeInsightXT  As SolidEdgeFramework.SolidEdgeInsightXT
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objSolidEdgeInsightXT = objApplication.SolidEdgeInsightXT

    Dim FileItemID As String
    Dim FileItemRevID As String
    Dim FileNames As Variant
        
    FileItemID = "020147"
    FileItemRevID = "A"
    
    Call objSolidEdgeInsightXT.GetListOfFilesFromInsightXTServer(FileItemID, FileItemRevID, FileNames, listoffiles)

    Set objSolidEdgeInsightXT = Nothing
    Set objApplication = Nothing
End Sub
See Also

SolidEdgeInsightXT Object  | SolidEdgeInsightXT Members  | Solid Edge ST4 - What's New