Solid Edge Framework Type Library
DeleteFilesFromCache Method
The variant array which contains the file list to be Deleted from Cache.
Description
Deletes files in the cache
Syntax
Visual Basic
Public Sub DeleteFilesFromCache( _
   ByRef psaCacheFiles() As Variant _
) 
Parameters
psaCacheFiles
The variant array which contains the file list to be Deleted from Cache.
Example
Private Sub Command1_Click()
    On Error Resume Next
    Dim objApplication As SolidEdgeFramework.Application
    Dim objSolidEdgeInsightXT  As SolidEdgeFramework.SolidEdgeInsightXT
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objSolidEdgeInsightXT = objApplication.SolidEdgeInsightXT

    Dim psaCacheFiles(1) As Variant
    varInputList(0) = "F:\020042.par"
    varInputList(1) = "F:\020043.asm"
    Call objSolidEdgeInsightXT.DeleteFilesFromCache(psaCacheFiles)

    Set objSolidEdgeInsightXT = Nothing
    Set objApplication = Nothing
End Sub
See Also

SolidEdgeInsightXT Object  | SolidEdgeInsightXT Members  | Solid Edge ST4 - What's New