Solid Edge Framework Type Library
AssignItemID Method
Item Type.
Returns the newly created Item Id.
Returns the newly created Item Rev.
Description
Generate the Item ID and Item RevisionID
Syntax
Visual Basic
Public Sub AssignItemID( _
   ByVal bstrItemType As String, _
   ByRef bstrItemId As String, _
   ByRef bstrItemRev As String _
) 
Parameters
bstrItemType
Item Type.
bstrItemId
Returns the newly created Item Id.
bstrItemRev
Returns the newly created Item Rev.
Example
Private Sub Command1_Click()
    On Error Resume Next
    Dim objApplication As SolidEdgeFramework.Application
    Dim objSolidEdgeInsightXT  As SolidEdgeFramework.SolidEdgeInsightXT
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objSolidEdgeInsightXT = objApplication.SolidEdgeInsightXT

    Dim FileItemRevID As String
    Dim FileItemItemID As String
    'Initialise the variables
    FileItemItemID = ""
    FileItemRevID = ""
    FileItemType = ""
    Call objSolidEdgeInsightXT.AssignItemID(FileItemType, FileItemItemID, FileItemRevID)
    
    MsgBox (FileItemItemID)
    MsgBox (FileItemRevID)

    Set objSolidEdgeInsightXT = Nothing
    Set objApplication = Nothing
End Sub
See Also

SolidEdgeInsightXT Object  | SolidEdgeInsightXT Members  | Solid Edge ST4 - What's New