Solid Edge Framework Type Library
RoutingSlip Object Members
Overview 
Public Methods
Public Method AddRecipientPlaces a person on the distribution of a routed document.
Public Method GetRouteInfoProvides the user interface to gather the information for routing the associated document.
Public Method ResetClears RoutingSlip and Accelerator objects. For CommandBar objects, returns the built-in command bar to a default configuration.
Public Method RouteDistributes the document according to the routing slip information.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property ApproveIndicates the current recipient's approval.
Public Property ApprovedIndicates whether or not the current recipient has approved or rejected the associated document.
Public Property AskForApprovalIndicates if an approval should be requested for each recipient.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DeliverySets and returns the delivery method used when routing.
Public Property HasRoutedSpecifies the current routing status of the referenced RoutingSlip object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property MessageSets and returns the message text for the referenced RoutingSlip object.
Public Property ParentReturns the parent object for the referenced object.
Public Property RecipientsSets the recipients on the referenced Routing Slip object.
Public Property ReturnWhenDoneDetermines whether or not the associated document is returned to the originator after completing its route.
Public Property StatusReturns the status of the specified object.
Public Property SubjectFor RoutingSlip objects, sets and returns the subject of the routing slip mail message. For SummaryInfo objects, sets and returns a general description of the associated document.
Public Property TrackStatusSpecifies whether or not tracking is to be activated for the referenced RoutingSlip object.
See Also

RoutingSlip Object