Solid Edge Framework Type Library
Reference Object Members
Overview 
Public Methods
Public Method GetMatrixReturns the transformation matrix for the referenced Occurrence or Reference object.
Public Method GetOccurrencesInPathMethod to get occurrences from Reference.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property ImmediateParentReturns the immediate parent for the referenced object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property ObjectReturns the dispatch interface associated with the site.
Public Property ParentReturns the parent object for the referenced object.
Public Property StyleFor collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Public Property TypeSpecifies the type of the object being referenced.
See Also

Reference Object