Imports System.Runtime.InteropServices
Public Class Form1
Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
Dim objApp As SolidEdgeFramework.Application = Nothing
Dim objType As Type = Nothing
Dim objMatTable As SolidEdgeFramework.MatTable = Nothing
Dim strLibrary As String = "Materials"
Dim objDocument As SolidEdgePart.PartDocument = Nothing
Dim strMaterial As String = "Copper"
Dim iMatPropIndex As SolidEdgeConstants.MatTablePropIndexConstants
Dim varGetPropVal As Object = Nothing
Dim strMessage As String
Try
' Get SE handle
objApp = Marshal.GetActiveObject("SolidEdge.Application")
If objApp Is Nothing Then
' Get the type from the Solid Edge ProgID
objType = Type.GetTypeFromProgID("SolidEdge.Application")
' Start Solid Edge
objApp = Activator.CreateInstance(objType)
' Make Solid Edge visible
objApp.Visible = True
End If
objDocument = objApp.Documents.Add("SolidEdge.PartDocument")
' Get material table object handle
objMatTable = objApp.GetMaterialTable()
' Set active document handle
objMatTable.SetActiveDocument(objDocument)
strMaterial = "ABS Plastic, high impact"
objMatTable.ApplyMaterialToDoc(objDocument, strMaterial, strLibrary)
iMatPropIndex = SolidEdgeConstants.MatTablePropIndexConstants.seMaterialName
objMatTable.GetMaterialPropValueFromDoc(objDocument, iMatPropIndex, varGetPropVal)
strMessage = String.Format("Material Name = {0}", varGetPropVal.ToString())
MsgBox(strMessage)
Catch ex As Exception
MsgBox(ex.ToString)
End Try
End Sub
End Class