Solid Edge Framework Type Library
Parent Property
Description
Returns the parent object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Parent As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLayers As SolidEdgeFramework.Layers
    Dim objParent As SolidEdgeDraft.Sheet
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the Layers collection object
    Set objLayers = objSheet.Layers
    ' Get the Parent property
    Set objParent = objLayers.Parent
    ' USER DISPLAY
    If Not objParent Is objSheet Then
        MsgBox ("Error in the Parent property")
    End If
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objLayers = Nothing
    Set objParent = Nothing
End Sub
See Also

Layers Collection  | Layers Members