Solid Edge Framework Type Library
ISEModelRecomputeEvents Object Members
Overview 
Public Methods
Public Method AfterFeatureIsAddedOccurs after a specified feature is added.
Public Method AfterFeatureIsModifiedOccurs after a specified feature is modified.
Public Method AfterRecomputeOccurs after the model recomputes.
Public Method BeforeFeatureIsDeletedOccurs when a specified feature is deleted.
Public Method BeforeModelIsDeletedOccurs before a specified model is deleted.
Public Method BeforeRecomputeOccurs before the associated model recomputes.
See Also

ISEModelRecomputeEvents Object