Solid Edge Framework Type Library
ISEAssemblyRecomputeEvents Object Members
Overview 
Public Methods
Public Method AfterAddOccurs after an item is added to either the Occurrences collection or the Relations3d collection.
Public Method AfterModifyOccurs after an occurrence in the assembly is moved.
Public Method AfterRecomputeOccurs after the model is recomputed.
Public Method BeforeDeleteOccurs when an item is about to be deleted from either the Occurrences collection or the Relations3d collection.
Public Method BeforeRecomputeOccurs before the associated model is recomputed.
See Also

ISEAssemblyRecomputeEvents Object