Solid Edge Framework Type Library
ISEAnimationEvents Object
Members 
Description
Animation events.
Remarks
A complete sample program written in C# is delivered in the Solid Edge Custom folder. The program is in the SolidEdgeMovieRecorder folder. The program demonstrates recording either the animation timeline, drag component or both. It combines all of the movie recording APIs as well as animation event handling.
See Also

ISEAnimationEvents Members