Solid Edge Framework Type Library
GetRotation Method
Specifies the display index (sequence number in which the linear element was created) for the linear element.
Description
Returns the rotation of the reference hatch line.
Syntax
Visual Basic
Public Function GetRotation( _
   ByVal nDisplayIndex As Long _
) As Double
Parameters
nDisplayIndex
Specifies the display index (sequence number in which the linear element was created) for the linear element.
See Also

HatchPatternStyle Object  | HatchPatternStyle Members