Solid Edge Framework Type Library
FillStyle Object Members
Overview 
Public Properties
Public Property ActiveSets and returns the name of the active style object.
Public Property ColorSets and returns the color in which the active object is drawn.
Public Property DescriptionReturns a user-specified description of the referenced object.
Public Property FillBackgroundSets and returns the background color of the referenced object.
Public Property FillColorSets and returns the color with which to fill the background of an object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PatternNameSets and returns the name of the active pattern.
Public Property PatternTypeSets and returns the type of pattern to apply to the referenced FillStyle object.
Public Property RotationFor OLE objects, specifies the angle at which the object is rotated along its major axis. For hatch lines, sets and returns the rotation angle used to display hatch lines.
Public Property SpacingSets and returns the distance between the primary hatch lines in a hatch pattern.
Public Property UnitsSets and returns the units in which the line width is defined.
See Also

FillStyle Object