Solid Edge Framework Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objDocuments As SolidEdgeFramework.Documents
    Dim lngCount As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Documents collection
    Set objDocuments = objApp.Documents
    'Add few more documnets
    objDocuments.Add progID:="SolidEdge.SheetMetalDocument"
    objDocuments.Add progID:="SolidEdge.DraftDocument"
    ' objDocuments.Add ProgID:="SolidEdge.AssemblyDocument"
    'Get the Documents count
    lngCount = objDocuments.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objDocuments = Nothing
End Sub
See Also

Documents Collection  | Documents Members