AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Center | This read-write Boolean property sets and returns whether the referenced DashStyle object represents a repeated pattern. The property is True if the pattern is not repeated, and False if the pattern is repeated. |
DashGapCount | Returns the number of dashes and gaps in the dash definition. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
PercentStartEndDash | This read-write Double property sets and returns the percentage of the first and last dash drawn for the referenced DashStyle object. |
Units | Sets and returns the units in which the line width is defined. |