Solid Edge Framework Type Library
OnCommand Method
Collapse All
Expand All
Solid Edge Framework Type Library
>
DISEAddInEvents Object
: OnCommand Method
The ID of the command for which the event is triggered.
Description
Occurs when the user selects the button for the associated add-in.
Syntax
Visual Basic
Public Sub OnCommand( _ ByVal
nCmdID
As Long _ )
Parameters
nCmdID
The ID of the command for which the event is triggered.
See Also
DISEAddInEvents Object
|
DISEAddInEvents Members