Solid Edge Framework Type Library
DISEAddInEventsEx Object Members
Overview 
Public Methods
Public Method OnCommandOccurs when the user selects the button for the associated add-in.
Public Method OnCommandHelpOccurs when the user requests help for the associated add-in.
Public Method OnCommandOnLineHelpOccurs when the user requests help for the associated add-in.
Public Method OnCommandUpdateUIOccurs when the user interface needs to be updated.
See Also

DISEAddInEventsEx Object