Solid Edge Framework Type Library
AssemblyRecomputeEvents Object Members
Overview 
Events
Public Event AfterAddOccurs after an item is added to either the Occurrences collection or the Relations3d collection.
Public Event AfterModifyOccurs after an occurrence in the assembly is moved.
Public Event AfterRecomputeOccurs after the model is recomputed.
Public Event BeforeDeleteOccurs when an item is about to be deleted from either the Occurrences collection or the Relations3d collection.
Public Event BeforeRecomputeOccurs before the associated model is recomputed.
See Also

AssemblyRecomputeEvents Object