Solid Edge File Properties Object Library
CreateCustonPropertySet Method
Description
Creates Custom Property Set
Syntax
Visual Basic
Public Sub CreateCustonPropertySet() 
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objPropertySets As SolidEdgeFileProperties.PropertySets = Nothing

        Try
            ' Create a new instance of PropertySets.
            objPropertySets = New SolidEdgeFileProperties.PropertySets
            objPropertySets.Open("C:\Part1.par", False)
            objPropertySets.CreateCustonPropertySet()
            objPropertySets.Save()
            objPropertySets.Close()
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objPropertySets Is Nothing) Then
                Marshal.ReleaseComObject(objPropertySets)
                objPropertySets = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IJPropertySets Collection  | IJPropertySets Members  | Solid Edge V20 - What's New  | Solid Edge V19 SP3 - What's New