Solid Edge Draft Type Library
GostWeldSymbols Property
Description
Returns the GostWeldSymbols collection object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property GostWeldSymbols As Object
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheets As SolidEdgeDraft.Sheets = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objGostWelds As SolidEdgeFrameworkSupport.GostWeldSymbols = Nothing
        Dim objGostWeld As SolidEdgeFrameworkSupport.GostWeldSymbol = Nothing
        Dim objLines As SolidEdgeFrameworkSupport.Lines2d = Nothing
        Dim objLine1 As SolidEdgeFrameworkSupport.Line2d = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
            objApplication.Visible = True
            objDocuments = objApplication.Documents
            objDraftDocument = objDocuments.Add("SolidEdge.DraftDocument")
            objSheet = objDraftDocument.ActiveSheet
            objLines = objSheet.Lines2d
            objGostWelds = objSheet.GostWeldSymbols

            'Add a horizontal line
            objLine1 = objLines.AddBy2Points(0.1, 0.1, 0.3, 0.1)

            'Create GOST weld
            objGostWeld = objGostWelds.AddByTerminator(objLine1, 0.125, 0.1, 0.0, True)

            objGostWeld.AddVertex(0.2, 0.05, 0)

            'Set the properties for GOST weld symbol.
            objGostWeld.TextScale = 10
            objGostWeld.Leader = True
            objGostWeld.BreakLine = True
            objGostWeld.PermanentJoint = True
            objGostWeld.PermanentJointType = SolidEdgeFrameworkSupport.DimGostWeldPermanentJointTypeConstants.igDimGostWeldPermJointStitch
            objGostWeld.AboveBreakLineText = "Text Above"
            objGostWeld.BelowBreakLineText = "Below"
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Sheet Object  | Sheet Members  | Solid Edge ST3 - What's New