Solid Edge Draft Type Library
IsAlternatePosition Property
Description
Specifies whether or not this ModelMember represents an alternate position of an alternate position assembly..
Property type
Read-only property
Syntax
Visual Basic
Public Property IsAlternatePosition As Boolean
Remarks
If it is true, this model member represents an alternate view table.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing
        Dim objModelMembers As SolidEdgeDraft.ModelMembers = Nothing
        Dim objModelMember As SolidEdgeDraft.ModelMember = Nothing
        Dim bIsAlternatePosition As Boolean

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objDraftDocument = objApplication.ActiveDocument
            objSheet = objDraftDocument.ActiveSheet
            objDrawingViews = objSheet.DrawingViews
            objDrawingView = objDrawingViews.Item(1)
            objModelMembers = objDrawingView.ModelMembers
            objModelMember = objModelMembers.Item(1)
            bIsAlternatePosition = objModelMember.IsAlternatePosition

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

ModelMember Object  | ModelMember Members  | Solid Edge ST5 - What's New