Solid Edge Draft Type Library
GetMargins Method
Description
Margins for print. Margin is give in Units (igDraftPrintMillimeters or igDraftPrintInches). Only valid when SheetsPerPage = igMultipleSheets.
Syntax
Visual Basic
Public Sub GetMargins( _
   ByRef pdLeft As Double, _
   ByRef pdTop As Double, _
   ByRef pdRight As Double, _
   ByRef pdBottom As Double _
) 
Parameters
pdLeft
pdTop
pdRight
pdBottom
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
        Dim objDraftPrintUtility As SolidEdgeDraft.DraftPrintUtility = Nothing
        Dim left As Double
        Dim top As Double
        Dim right As Double
        Dim bottom As Double

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objDraftDocument = objApplication.ActiveDocument
            objDraftPrintUtility = objApplication.GetDraftPrintUtility()
            objDraftPrintUtility.Units = SolidEdgeDraft.DraftPrintUnitsConstants.igDraftPrintInches
            objDraftPrintUtility.AddDocument(objDraftDocument)
            objDraftPrintUtility.SheetsPerPage = SolidEdgeDraft.DraftPrintSheetsPerPageConstants.igMultipleSheets
            objDraftPrintUtility.SetMargins(1.5, 1.5, 1.5, 1.5)
            objDraftPrintUtility.GetMargins(left, top, right, bottom)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

DraftPrintUtility Object  | DraftPrintUtility Members  | Solid Edge ST3 - What's New