Solid Edge Draft Type Library
BestFit Property
Description
Scale sheet so that it fills selected paper size. The scale cannot exceed 1.0. Only valid when SheetsPerPage = igSingleSheets. SingleSheetScale is ignored if this property is true.
Property type
Read-write property
Syntax
Visual Basic
Public Property BestFit As Boolean
See Also

DraftPrintUtility Object  | DraftPrintUtility Members  | Solid Edge ST3 - What's New